Intente buscar por palabras clave, código de producto/pedido o número de serie, por ejemplo, "CM442" o "información técnica"
Introduzca por lo menos 2 caracteres para iniciar la búsqueda.
  • Historial

Scale up faster in fine chemicals without losing process understanding

Continuous, real‑time insight from lab experiments through full‑scale production preserves process knowledge, enabling earlier decisions, predictable scale up, and faster product release in fine and specialty chemical manufacturing.

Evonik installed Raman PAT in the chemical industry
Introduction

Where process understanding is lost in fine chemical scale-up

In fine chemicals development, the greatest delays and inefficiencies rarely originate in chemistry itself. They arise when moving the process between scales — when insights gained in the laboratory are not transferred reliably to pilot and production environments. Instead of building continuously on what is already known, teams are forced to reconstruct understanding at each phase and streamline production.

Off-line analytics, manual sampling, and phase‑specific model re-validation force teams to:

  • Repeat experiments during scale‑up
  • Rediscover operating windows at production scale
  • Delay product release while deviations are investigated
  • Absorb waste, rework, and additional development cost

When analytical insight breaks between lab, pilot, and plant, scale‑up becomes iterative instead of engineered.

Insight

What stays visible across lab, pilot, and production

Inline process analytical technologies (PAT), such as Raman spectroscopy, embeds chemical insight at the point where reactions and transformations actually occur — in laboratory reactors, pilot vessels, and production equipment. The same Raman probes and analytical models are applied directly in the process stream, generating continuous, in‑situ measurements at each scale. This makes process behavior visible inside the equipment itself, rather than being reconstructed from external lab analyses.

Across scales, Raman spectroscopy keeps critical process insights visible, such as:

  • Reaction progress and key chemical transformations
  • Process variability under real operating conditions
  • Deviations as they occur, not after losses accumulate
  • The validity of development models when transferred to production

Because Raman spectra often allow isolated peaks to be assigned to individual substances, multiple components can be simultaneously measured with a single spectrum. Information-rich spectra provide deep process insight and reduce scale-specific model re-calibration effort. Quantitative results are obtained faster — a critical advantage during development and scale‑up.

How continuous insight accelerates development and scale‑up decisions

When the same analytical measurements and models are applied consistently across lab, pilot, and production, decision‑making fundamentally changes. Teams no longer validate outcomes retrospectively; they act while experiments and trials are still running.

Lab-to-process analysis scalability enables:

  • Faster, evidence‑based decisions during development
  • Earlier confirmation of scale‑up readiness
  • Immediate intervention when conditions drift
  • Reuse of analytical models instead of rebuilding them
  • Replacement of slow, error‑prone manual sampling

The value is not more data, but in decision‑grade insight that remains consistent across scales.

German BASF Citral fine chemical plant ©Endress+Hauser
Action

Engineered continuity from lab to process

In fine chemicals manufacturing processes, performance and time‑to‑market are most at risk when process understanding breaks between lab, pilot, and production. By applying continuous, real‑time analytics across all phases, inline Raman spectroscopy establishes engineered continuity from development through manufacturing for critical process parameters and consistent product quality.

Analytical technology models are validated in the lab reactor, confirmed in pilot equipment, and enforced at production scale using the same measurement principle at the process interface. This removes uncertainty at the most critical transition points and enables predictable scale‑up, faster product release, and stable production performance by design — not by repeated iteration.

How lab insights become plant reality

Continuous lab‑to‑process real-time monitoring is realized through:

  • Inline Raman spectroscopy deployed as process analytical technology
  • Process analytical technologies reused consistently from R&D to production
  • Simultaneous monitoring of multiple measurement points for critical process parameters
  • Chemometric evaluations performed directly on the device in real time
  • Operation in demanding and ATEX‑rated environments

Rather than rebuilding understanding at each scale, insights are preserved and reused — creating a single, reliable analytical foundation across the production lifecycle.

Measurable value

From development insight to measurable production impact

In fine chemicals operations, fragmented insight translates directly into longer development cycles, higher waste, and slower market entry. Continuous lab‑to‑process analytical technologies convert development intent into operational reality.

Producers can demonstrate:

  • Faster process understanding and reduced time‑to‑market
  • Fewer scale‑up surprises and less rework
  • Lower raw‑material and energy consumption through targeted optimization
  • Higher throughput using existing assets
  • Safer, more compliant operation through reduced manual intervention

These outcomes are realized before production losses occur, not corrected afterward.

Two employees looking at installed Endress+Hauser Raman probes at the Evonik fine chemical plant ©Endress+Hauser
Case study

Proven at production scale: Evonik

Evonik demonstrates how continuous analytics transform fine chemicals development and manufacturing. By replacing manual sampling with inline Raman spectroscopy and deploying the same analytical models from R&D to production, process understanding is preserved through scale‑up and translated directly into safer, more efficient operation.

What Evonik can demonstrate in practice:

  • Seamless transfer of analytical models from development to production
  • Real‑time monitoring replacing slow, error‑prone manual sampling
  • Reduced calibration effort and faster quantitative results
  • Improved safety and operational efficiency, including in ATEX zones
  • Faster process understanding and reduced time‑to‑market

With over 50 measurement points and 16 Raman analyzers deployed globally, this approach shows how continuous analysis enables scalable, reliable manufacturing.

Dr. Andreas Ohligschläger at Evonik

"With Raman spectra, you might be able to assign isolated peaks to individual substances in the mixture. This significantly reduces the calibration effort and quickly leads to quantitative results."

Dr. Andreas Ohligschläger, PAT Engineer, Evonik Industries AG
Our expertise

Why Endress+Hauser?

Endress+Hauser helps fine and specialty chemicals manufacturers engineer predictable, scalable processes by embedding process analytical technology directly into development and production workflows.

  • Deep expertise in chemical and specialty processes
  • Robust Raman systems for demanding environments
  • Strong application engineering and global project experience
  • Long‑term service partnerships ensuring continuity and reliability

From early development to full‑scale production, we ensure that what is learned in the lab becomes a repeatable, reliable part of daily operation.

Operational rollout

What questions should we ask when considering Raman spectroscopy?

Review the questions and decision criteria process engineers use to assess Raman technology adoption readiness, before committing time and resources to implementation.

Product highlights 

Explore our Raman spectroscopy systems

/
FAQ

Everything you need to know 

Next steps

Contact

Discuss your process challenges with our chemical industry experts. We are here to support you.

Notas al pie

Might also interest you